Configure the Network Parameters

When the Connection Type is set to MPI via serial adapter, use these fields on the Connection tab(s) to configure the Network Parameters:



Disclaimer

ClearSCADA 2017 R2