Configure the Set Value Action

When you use, for example Function Block Diagrams or an OPC-DA client, to set the value of an output point, the Set Value Action combo box on the Control tab allows you to define how point values are set. This only applies to Analog or Digital output points. The options available are defined by the outstation protocol.

Outstation using the LACBUS-RTU protocol

Select the Set Value Action combo box to define what action is performed:

Outstation using the SOFBUS-PL protocol

Select the Set Value Action combo box to define what action is performed:


Disclaimer

ClearSCADA 2017 R2