Configuring the Direct Tab
Sofrel outstations do not support continuous direct online communications. Direct and Shared outstations include a Direct tab that provides a Direct Communications Connection section. This section allows you to configure the availability of the outstation’s direct connection.
The following fields define how ClearSCADA manages the direct communications with the Sofrel outstations:
Direct and Shared outstations are always On Demand. This check box is permanently selected, grayed out and cannot be changed.
Enter the maximum number of times that the ClearSCADA server will re-attempt to request data from the outstation.
If the outstation fails to respond to the server’s initial data request, the server will make a further request (referred to as a ‘retry’). The server can repeat a data request up to the defined number of Retries.
If the outstation still fails to respond once the number of Retries has been exhausted, ClearSCADA will deem the permanent connection to the outstation to have failed. If the outstation has a dial-up modem as a backup means of communication, the server will then attempt to dial out to the outstation to request the data via PSTN.
Enter the time that the server will wait before attempting a ‘retry’. This delay is useful, as an immediate retry is likely to fail for the same reason as the previous attempt.
Enter the duration in the OPC Time Format. The default of 30 seconds is suitable for many systems.
Specify the maximum amount of time for which the direct connection is to remain online. Enter the duration in the OPC Time Format.
ClearSCADA terminates the connection as soon as it has retrieved the outstation’s data, or once the Max Online Time is reached, whichever is the shorter, unless:
- The Close Connection pick action is used to close the open connection.
- The Extend Connection pick action is used to extend the time for which the open connection remains online.
- The Open Connection pick action is used to trigger communications with the outstation. An Open Connection keeps the connection open for the whole of the Max Online Time, even after any data retrieval is complete, unless either of the pick actions mentioned above are executed.
By default, ClearSCADA logs several messages in the Event Journal when establishing communications with an outstation. Several of these messages are assigned an 'Outstation Comms' category.
Select this check box if ClearSCADA is only to log 'Outstation Comms' category messages when it first successfully opens a direct connection with the outstation. For each subsequent direct connection that proves successful, ClearSCADA only logs messages relating to the command that caused ClearSCADA to open that direct connection (for example, 'Open connection requested' and 'Open connection request successful'). The exception to this is if a connection attempt proves unsuccessful—on the next successful connection, ClearSCADA will log the relevant 'Outstation Comms' category messages as well as messages relating to the command that caused ClearSCADA to open the direct connection.
Clear the 'Suppress Connection Logging' check box (the default) if ClearSCADA is to log the relevant 'Outstation Comms' and command-related messages whenever it successfully opens a direct connection with the outstation. 'Outstation Comms' category messages might include, for example, 'Starting comms...', 'Connecting...', 'Established comms...'
, and 'Communications state - Healthy...'
messages.
By default, ClearSCADA logs several messages in the Event Journal should its attempts to establish communications with an outstation prove unsuccessful. Several of these messages are assigned an 'Outstation Comms' category.
Select this check box if ClearSCADA is only to log 'Outstation Comms' category messages following its first unsuccessful attempt to open a direct connection with the outstation. For each subsequent attempt to open a direct connection that proves unsuccessful, ClearSCADA only logs messages relating to the command that caused ClearSCADA to attempt to open that direct connection (for example, 'Open connection requested' and 'Open connection request failed'). The exception to this is if a connection attempt succeeds—on the next unsuccessful connection attempt, ClearSCADA will log the relevant 'Outstation Comms' category messages as well as messages relating to the command that caused ClearSCADA to attempt to open the direct connection.
Clear the 'Suppress Failed Connection Logging' check box (the default) if ClearSCADA is to log the relevant 'Outstation Comms' and command-related messages whenever its attempts to open a direct connection with the outstation prove unsuccessful. 'Outstation Comms' category messages might include, for example, 'Starting comms...', 'Connecting...', 'Communications state - Failed', and 'Communications state - Disconnected' messages.