Sofrel Call Recipients

Sofrel S500 series outstations that are configured to use the LACBUS-RTU protocol can be configured to use a list of Call Recipients. The list is used by the outstation to initiate communications with one or more of the recipients configured.

There are several defined types of call recipients supported by Sofrel outstations:

These recipient types are identified in the outstation, the type is not uploaded to ClearSCADA.

ClearSCADA recipient type restrictions

The following restrictions apply to how ClearSCADA manages recipient types:


Disclaimer

ClearSCADA 2017 R2