File Locations (Default)

ClearSCADA installs files in several locations. Some of these files you may need to access during the configuration of your system and so you should familiarize yourself with the default locations.

The following sections detail the default file locations for ClearSCADA on the following Windows platforms:

These are the default file locations—the files on your system may be in different locations, depending on how the system has been installed and configured.

If you cannot locate a file at the default location, check the file's location using the Server Administration Tool, or use the Search facility in Windows.

You can change the location of the server files by using the Server Administration Tool. For more information, see Locations of the Database Folders in the ClearSCADA Guide to Server Administration.

You can change the location of log files by using the Move Log Files wizard (see Move all New Log Files to a Different Location in the ClearSCADA Guide to Server Administration).


Disclaimer

ClearSCADA 2017 R2