Run the ClearSCADA WebX Server Installer

To install the ClearSCADA Web Server, you need to run the ClearSCADA installer program.

To run the ClearSCADA installer:

  1. Insert the ClearSCADA DVD. If Autorun is disabled on your PC, run the DVD manually.
  2. When the ClearSCADA screen is displayed, select the Install ClearSCADA Web Server option.

    The ClearSCADA Web Server installer runs.

  3. When you run the ClearSCADA installer, Windows may ask you if you want ClearSCADA Setup to be able to make changes to your computer. Choose Yes to allow the ClearSCADA installation to continue.

The Welcome ‘page’ is shown (see WebX Server Setup Wizard).

If your PC does not have the prerequisite components, the ClearSCADA installer will attempt to install them before installing ClearSCADA (see Installation of Prerequisites).


Disclaimer

ClearSCADA 2017 R2