Uninstalling ClearSCADA

There are two different ways of uninstalling ClearSCADA:

To discover which of the uninstall processes is most appropriate for your requirements, answer the questions below:

  1. Do you intend to re-install ClearSCADA on the computer at a later date?
  2. Do you want a re-installed version of ClearSCADA to use only the default settings (that is, be a ‘clean’ install)?

If you answered no to any of the questions, we recommend that you use the ‘Quick’ uninstall process (see Uninstall ClearSCADA - ‘Quick’ Uninstall).

If you answered yes to both of these questions, you should use the ‘Complete’ uninstall process (see Uninstall ClearSCADA - ‘Complete’ Uninstall). But to do so, you need to have experience of editing registry settings in Windows. This is because incorrect configuration of the registry can cause serious problems with the Windows operating system.

To perform a complete uninstall, you need to also uninstall the ClearSCADA WebX component, which is installed separately from ClearSCADA, (see Uninstall ClearSCADA WebX - 'Quick' Uninstall).


Disclaimer

ClearSCADA 2017 R2