Upgrading a License
You need to upgrade your ClearSCADA license(s) as part of the ClearSCADA upgrade process. The license(s) affect which features, drivers, and so on, are available on your system.
There are two types of ClearSCADA license:
- a dongle license (which is stored on a USB dongle device)
- a software license (which is a file that can be sent to you electronically or downloaded).
The technique you use to upgrade your ClearSCADA license will vary depending on the type of license you use. For more information, please refer to the section that is relevant to your ClearSCADA system, see the topics that are listed in the gray footer section at the bottom of this topic. Select the relevant entry to display the topic that you require.