The Navigation Bar and Window Layout

Once you are logged on as the 'EngExample' user, the WebX window refreshes. The Alarm Banner is displayed at the bottom of the window, and the Database Bar is displayed to the left of the document display area. A Mimic called 'Opening Page' is displayed in the document display area. The Mimic displays automatically in WebX whenever you log on as the 'EngExample' user. You can also access the Mimic in ViewX. The Mimic displays automatically because the 'EngExample' user account is associated with a home page. In the configuration of the 'EngExample' user account, the 'Opening Page' Mimic is specified as the Home Page.

The navigation bar at the top of the WebX window contains buttons that provide access to various displays and Explorer Bars:

You will use some of the navigation bar buttons later in this tutorial.

As the WebX interface is responsive, depending on the size of the WebX window, the navigation bar might contain icons, rather than named commands:

If you are unsure which option a particular icon represents, place the cursor over the icon and look at the text that appears in the status bar at the bottom of the WebX window.

 

Now that you have logged on, you can use the WebX interface to operate your system. Proceed to Use the Alarm Banner on a WebX Client.

Further Information

Understand WebX: see WebX Client in the ClearSCADA Guide to ViewX and WebX Clients.

Use the Systems Toolbar in the ClearSCADA Guide to ViewX and WebX Clients.


Disclaimer

ClearSCADA 2017 R2