Define the Point Scaling

Use the fields in the Scaling section of the TBox Analog Input Point or TBox Analog Output Point Form to specify the type and range of the raw input signals, so that they can be suitably converted into floating-point engineering values for use in the ClearSCADA database.

The scaling is also used on the TBox Analog Output Point to perform a similar conversion on any output signals. ClearSCADA uses the conversion calculation to produce a raw data value that is sent to plant.


Disclaimer

ClearSCADA 2017 R2