Digital Point Tab

Display the Properties window for a Totalflow Digital Point item and then select the Digital Point tab. The property of interest on this tab is the Number of Bits setting.

When the TreatValueAsBitfield option on the Options tab is clear, the value of the Number of Bits field has to be 1. As such, the Digital Point can only have valid values of 1 or 0. Control is limited to writing a new value of 1 or 0.

When the TreatValueAsBitfield option on the Options tab is selected, the value of the Number of Bits field can be from 1 to 3, which means that Digital Point can have a value of 0 to 7. Control can span the entire range of 0 to 7. Additionally, you can use the Offset field to write bits at an arbitrary location in the value.

Further Information

Defining Digital Point Details in the ClearSCADA Guide to Core Point Configuration.

Tabs on Point Forms in the ClearSCADA Guide to Simple Drivers.


Disclaimer

ClearSCADA 2017 R2