Events Group

The example project includes an Events group.

The Events group contains a Data Table (TotalflowEvents) to hold events from the Totalflow. This is the table that is referenced on the Scanner tab of the ScannerDaily object. If you manually create your own Data Table to hold events, as opposed to having the driver do it for you automatically, you can optionally use the schema from this Data Table as a starting point.

The Logic subgroup contains some very simple scripts that can be used to manipulate the contents of the Data Tables. These scripts are called from pick actions on the EventsAndAlarms Mimic.

Further Information

Event Data Table.


Disclaimer

ClearSCADA 2017 R2