How can I change the orifice plate diameter for a tube run?
To read the orifice plate diameter, set up a Totalflow Numeric Point to read Array = 7 and Register = 8. Set the Application number to that of the application for which you want to change the orifice plate. Enable the Control aggregate on the point. To change the value, call the Control method on the Control aggregate for the point (see Numeric Point Control Tab).
Further Information