Scanner Methods
- CancelPromotedScanning—This method lets you manually exit the Promoted Scanning mode. When this method is called, the scanner is configured to use the normal scanning rate and offset that are found on the scanner’s configuration form. The method takes no parameters.
- ChangeGasComp—This method lets you change the gas composition that is used in the AGA-8 (compressibility) calculation in the Totalflow. This method takes the gas composition parameters and then sets them all in the Totalflow in a single transaction.
This method is also available as a pick action. As such, if your user account has the relevant permissions, you can right-click on a Totalflow Scanner object in the Database Bar, and then select the Change Gas Composition pick action. The Change Gas Composition window is displayed.
The parameters that you need to specify are listed in the table below. The parameters are listed in the order in which they need to appear in the method call. Use the App Number field to specify the number of the Application in the Totalflow for which you want to change the gas composition.
Select the Live Composition check box to change the Live Analysis Data in the Totalflow device, instead of the Fixed Analysis Data.
If you select the Normalize option, the non-zero gas composition values are adjusted in equal proportion so that so that the sum of all of the elements equals 100. The method call/pick action will be unsuccessful if the individual gas composition values do not sum to 100 and the Normalize option is not selected.
The driver does not automatically update the points that monitor the gas composition after the ChangeGasComp method is called. You will either need to call the Refresh method on the Totalflow Scanner, or wait for the next poll for points to be updated.
|
Parameter Name |
Number |
Fixed Array.Index |
Live Array.Index |
Type |
Unit |
|---|---|---|---|---|---|
|
App Number |
1 |
|
|
byte |
none |
|
Live Composition |
2 |
|
|
bool |
none |
|
N2 nitrogen |
3 |
3.21 |
3.46 |
double |
percent |
|
CO2 carbon dioxide |
4 |
3.22 |
3.47 |
double |
percent |
|
H2S Hydrogen Sulfide |
5 |
3.23 |
3.48 |
double |
percent |
|
H2O Water |
6 |
3.24 |
3.49 |
double |
percent |
|
He Helium |
7 |
3.25 |
3.50 |
double |
percent |
|
CH4 Methane |
8 |
3.26 |
3.51 |
double |
percent |
|
C2H6 Ethane |
9 |
3.27 |
3.52 |
double |
percent |
|
C3H8 Propane |
10 |
3.28 |
3.53 |
double |
percent |
|
C4H10 n-Butane |
11 |
3.29 |
3.54 |
double |
percent |
|
C4H10 i-Butane |
12 |
3.30 |
3.55 |
double |
percent |
|
C5H12 n-Pentane |
13 |
3.31 |
3.56 |
double |
percent |
|
C5H12 i-Pentane |
14 |
3.32 |
3.57 |
double |
percent |
|
C6H14 n-Hexane |
15 |
3.33 |
3.58 |
double |
percent |
|
C7H16 n-Heptane |
16 |
3.34 |
3.59 |
double |
percent |
|
C8H18 n-Octane |
17 |
3.35 |
3.60 |
double |
percent |
|
C9H20 n-Nonane |
18 |
3.36 |
3.61 |
double |
percent |
|
C10H22 n-Decane |
19 |
3.37 |
3.62 |
double |
percent |
|
O2 Oxygen |
20 |
3.38 |
3.63 |
double |
percent |
|
CO Carbon Monoxide |
21 |
3.39 |
3.64 |
double |
percent |
|
H2 Hydrogen |
22 |
3.40 |
3.65 |
double |
percent |
|
Ar Argon |
23 |
3.41 |
3.66 |
double |
percent |
|
Normalize |
24 |
|
|
bool |
N/A |
- EnablePromotedScanning—Use this method to temporarily change the scanning rate on a Scanner object. The method takes a single input parameter: Promoted Scan Duration. The units for this parameter are seconds. Use the Promoted Scan Duration parameter to define the length of time that the Scanner object will be configured to use the Promoted Scan Rate. The scanner exits promoted scanning mode automatically once the Promoted Scan Duration expires; alternatively, promoted scanning mode can be exited manually by calling the CancelPromotedScanning method.
- ResetCommCounters—Use this method to clear the communications counters that are mentioned in the section on Scanner Data Fields. The method takes no parameters.
- ResetNewestEventTimes—Use this method to reset the values in the NewestEventTimes tag. The method is useful if you want to re-scan the Event Data Table from the Totalflow device. To reset all of the newest event times, call this method with a parameter of 0. To reset just a single value, call this method with the tube number for which you want to reset the NewestEventTime.
- SetClock—Use this method to set the clock in the Totalflow device to the local time at the ClearSCADA host. The method takes no parameters.
Further Information