Trend Point Data Fields

In addition to the usual data fields that you would expect to find on a ClearSCADA Point object, a Totalflow Trend Point object also has the following data fields, which are listed in the ClearSCADA Database Schema (Trend Point Schema View). The name in bold at the start of each entry is also the OPC tag name.

Further Information

Trend Point Schema View


Disclaimer

ClearSCADA 2017 R2