String

A string has to be enclosed within single straight quotation marks, in the format:

<Identifier> = '<string>'

Any string that references an item in the database is case sensitive.

Where a string is to evaluate as an expression:

Any string used in the expression has to be enclosed in two sets of single straight quotation marks.

Any OPC tag or string that references an item in the database is case sensitive.

For more information on the syntax you can use to reference an item in the database, see Syntax of OPC Property Tags.


Disclaimer

ClearSCADA 2017 R2