SID
Many of the series of Trio radios with which ClearSCADA can communicate provide SID support.
The Stream Identifier code (also known as the Stream ID or SID code) provides the addressing mechanism for data stream routing on radio networks that use multiple message streams. The SID code identifies the message stream that is used by a particular Trio radio on such a radio network.
ClearSCADA provides these configuration properties related to SID support:
- The Send SID check box on the Trio Diagnostics Channel Form (see Specify Whether to Include the Stream Identifier in each Data Packet)
- The Stream ID field on each Trio Diagnostics Radio Form (see Specify the Stream on which the Radio is to Transmit Messages).
For further information on SID codes and multistream functionality, see the documentation supplied with your Trio radio equipment.