How Do I Display 'Popup' Content as a Normal Help Page?

Some topic hyperlinks display the target file in a popup window. Popups are used to display related information without taking you away from the source topic, or interrupting your topic viewing sequence. When you close the popup window (by clicking elsewhere within the help's document display area), you remain on the help topic from which you displayed the popup window.

Occasionally, you might want to view the popup content in place of the source topic. If so, check whether the popup content appears as a link elsewhere in the topic - for example, in the topic footer, or in a 'Further Information' section at the end of the topic. Such links typically take you from the source topic to the target topic.

Alternatively, copy the heading from the topic in the popup window, and paste it into the search field in the Help window. Enclose the search string within double quotation marks. (You might want to view the topic's path in the topic header in the popup window, in case more than one topic has the same topic heading.) Close the popup window and perform the search. Select the relevant topic from the list of search results.


Disclaimer

ClearSCADA 2017 R2