Alarm Response

Associated with: Any item for which an alarm can be raised

Security permission required to access this option: Acknowledge Alarms

Select this option on the Object Menu to indicate that you are aware of an alarm without acknowledging it (see Respond to an Alarm).

If using this pick action with the Automation Interface, you need to specify the method name SetAlarmResponse.

Also see Acknowledge Alarms.


Disclaimer

ClearSCADA 2017 R2