Disabled Alarms

Associated with: Groups and Group Instances

This status attribute indicates the total number of items within the Group or Group Instance (including any subgroups) that have their alarms disabled.

Example:

6

Alarms are disabled using the Disable Alarms pick action (see Disable Alarms). When an item’s alarms are disabled, that item’s entry on any ClearSCADA displays such as Queries Lists uses the Alarm Disabled color (unless another system color takes priority over that color). The individual item’s Alarm State status attribute also indicates whether the item’s alarms are disabled.


Disclaimer

ClearSCADA 2017 R2