Enable Alarms

Associated with: Any item for which an alarm can be raised

Security permission required to access this option: Disable Alarms

The Enable Alarms option on the Object Menu is only available on database items that can have alarms. Access to the option is also dependent on the server configuration (which might restrict access to the option).

The Enable Alarms option allows you to enable (register), alarms for the selected item.

Select the option on an individual database item, such as a point, to enable the alarms on that particular item.

Select the option on a Group or Group Instance, to enable the alarms on the items in the Group or Group Instance and in any subgroups within that Group or Group Instance.

For more information, see Enable Alarms.


Disclaimer

ClearSCADA 2017 R2