Exclusive Control User

Associated with: All items that are under Exclusive Control

This status attribute is only displayed if the Exclusive Control feature is enabled on your system and an item is currently under Exclusive Control (see Exclusive Control).

The status attribute displays the name of the user that currently has Exclusive Control of the item.

Further Information

Take Complete Exclusive Control: see Taking Exclusive Control.

Take Partial Exclusive Control: see Taking Exclusive Control.

Release Exclusive Control: see Releasing Exclusive Control.


Disclaimer

ClearSCADA 2017 R2