Minimize the Ribbon

You can minimize the ViewX ribbon so that only the ribbon tabs are visible. This allows you to increase the space available for the document display area, while still providing access to the ribbon tabs.

To minimize the ribbon, either:

Or:

Or:

Or:

Or:

While the ribbon is minimized, only the ribbon tabs are visible. The rest of the ribbon contents are hidden.

If you display ViewX in Full Screen mode, the ribbon is automatically minimized and the Quick Access Toolbar is also hidden. For more information about Full Screen mode, see View Tab.

To view the contents of a particular tab, click on the required tab. The ribbon contents for the selected tab remain visible until you click elsewhere within the ViewX client.


Disclaimer

ClearSCADA 2017 R2