Understanding Your System

You can use ViewX (the primary ClearSCADA Man-Machine Interface) or a WebX client to operate your ClearSCADA system. Before you begin to work with either of the interfaces, you need to understand the principles of your system and some of the terminology used in ClearSCADA. By learning about these basic concepts, you will develop an understanding of how your system works and how your actions will affect the system.

To learn about the basic concepts of a ClearSCADA system, see these sections:

For further information on the types of ClearSCADA client you might use, see ViewX Client, and see WebX Client.

For information on the types of driver that might be installed on your system, and for an overview of master-slave setups, and direct and PSTN communications, see Welcome to the ClearSCADA Guide to.

For information on the terminology used throughout this guide, see Terminology.


Disclaimer

ClearSCADA 2017 R2