View the System Status on a WebX Client

You can view basic information about the ClearSCADA server to which the web server is connected. To do this:

  1. Select the Systems button on the navigation bar.
    The Systems toolbar is displayed.

  2. Select the System Status button .
    The System Status page is displayed.

    Information shown includes:

    • The name of the ClearSCADA Server to which the web server is connected
    • The State of the server (typically 'Main' or 'Standby')
    • The date and time that the server last changed state.

Further Information

Use other options on the Systems toolbar: see Use the Systems Toolbar.

View an Item’s Status on a WebX Client.


Disclaimer

ClearSCADA 2017 R2