Configure Most Settings using the Configuration Application

If you want to use a vendor-supplied Configuration Application to configure most or all of the incremental configuration settings, you can use the following strategies:

Your Field Device may have integrated configuration features or other configuration tools that you can use instead of the Configuration Application.


Disclaimer

ClearSCADA 2017 R2