Configure a WITS Pulse (NULL) Action
Use the fields within the Actions section of the Pulse (NULL) tab to define the properties of the NULL pulse action. For more information, see Configure a NULL Pulse Action.
In the DNP3 WITS Driver, you can also set the following property for the NULL action:
- Point Number—Enter the DNP3 point number that uniquely identifies the binary output point in the outstation to which you want ClearSCADA to send the pulse action.