Export Image
Associated with: WITS Firmware Images.
Security permission required to access this pick action: Configure.
You can use the Export Image action to export the firmware image file from ClearSCADA. The firmware image file can then be used in external applications.
When you select Export Image, a browse window is displayed - select a suitable location for the export file and enter a suitable filename, and then select OK.