General Point Properties - WITS Maximum Points

Use the fields at the top of the Maximum tab to Configure General Point Properties.

The following field is specific to the WITS driver:


Disclaimer

ClearSCADA 2017 R2