Health Check Status

Associated with: WITS Outstations.

 

WITS Field Devices can send health check status information to ClearSCADA for the following attributes:

 

After ClearSCADA has first communicated with the Field Device:

 

When the status of a health check attribute changes, ClearSCADA may log the details in the Event Journal (if logging is enabled) (see Understand Events Lists in the ClearSCADA Guide to Lists). ClearSCADA may also raise an alarm (see Understand Alarms and see Define the Severity for Health Check Logging).


Disclaimer

ClearSCADA 2017 R2