Uploading and Downloading (WITS)

Some WITS Field Devices support one or more of the following:

This is defined in the Device Profile for each Field Device (see WITS Device Profiles).

Depending on the capabilities of your Field Device, you may be able to use ClearSCADA to upload or download:


Disclaimer

ClearSCADA 2017 R2