WITS-Specific Driver Log File Options

This section is for system administrators and high-level engineers who need to use diagnostic information to assess the state of the ClearSCADA system. Use this section in conjunction with the DNP3 driver documentation (see System Analysis).

This section gives details of the logging options that are available to the DNP3 WITS driver.

To determine which logging options are available, select the DNP3 driver option from the Modules section of the ClearSCADA Server Status Tool, then select the Logging option to display the DNP3 Logging window.

For more information on driver logging, and for information on the DNP3 driver logging options that are available to this DNP3 extension driver, see Driver Logging Options that are Specific to the DNP3 Driver,.


Disclaimer

ClearSCADA 2017 R2