EngineeringUnit

Description

The unit of measure for an analog tag. For example: mph, grams, or pounds.

ClearSCADA Metadata Field

WH_EngineeringUnit

Default Value

This will usually be the Units configured for the point or accumulator. For points that don't have units (for example, digital points) the default is an empty string.

Type

String.


Disclaimer

ClearSCADA 2017 R2