IntegralDivisor

Description

The integral divisor that is associated with the engineering unit for the tag. The integral divisor is the factor Wonderware Historian applies when it integrates a rate with the units [EngUnits/TimeUnit] to a quantity with units [EngUnits]. A value of 1 assumes a time unit of seconds and ensures that a rate of [Unit/second] is correctly integrated to [Unit]. For a time unit of minutes, set the integral divisor value to 60; for a unit of hours, set the integral divisor value to 3600. Apply the integral divisor in a similar way to rates or quantities that are not expressed in terms of a time unit. For example, to convert watts to watt-hours, the integral divisor is 1/3600. To convert watts to kilowatt-hours, the integral divisor is 1/3600000.

ClearSCADA Metadata Field

WH_IntegralDivisor

Default Value

The default value is 0.

Type

Double.

 


Disclaimer

ClearSCADA 2017 R2