MinRaw

Description

The minimum value of the raw acquired value. This property applies to analog tags.

As ClearSCADA exports data that has already been scaled, additional scaling by Wonderware Historian should not be required. Therefore, ClearSCADA sets the value of the ApplyScaling property to False and so this property isn't applicable.

ClearSCADA Metadata Field

WH_MinRaw

Default Value

The default value for this property is 0.

Type

Double.

Further Information

ApplyScaling

MaxRaw

MaxEU

MinEU


Disclaimer

ClearSCADA 2017 R2