RateDeadBand

Description

The storage rate deadband for the tag. The rate deadband is the percentage of deviation in the full-scale value range for an analog tag. The swinging-door (rate) deadband applies to Delta storage only. You can use time and/or value deadbands in addition to the swinging-door deadband. You can use any value greater than 0 for the deadband. A value of 0 indicates that Wonderware Historian will not apply a swinging-door deadband. In ClearSCADA the TagStorageType is always set to Forced, and therefore this property is not applicable.

ClearSCADA Metadata Field

WH_RateDeadBand

Default Value

The default value for this property is 0.

Type

Double.

 


Disclaimer

ClearSCADA 2017 R2