Current Connection

The Current Connection attribute indicates which connection is the current network connection between eDNALinkMx and the Wonderware eDNA Historian server.

The possible connections are: Primary or Secondary.

For more about the primary and secondary connections, see Specify the Connection Properties


Disclaimer

ClearSCADA 2017 R2