Reinstate the Default Settings for an X-Y Plot

If you have used the Go To Time feature (see Move to a Specific Time on an X-Y Plot), you may have set the X-Y Plot’s Time Line to display a different amount of time than is specified in the Time Line’s configuration. You can reset the X-Y Plot to reinstate the default settings (defined in the Time Line’s configuration) at any time by using the Revert to Defaults option.

To reinstate the default settings for an X-Y Plot:

  1. Display an X-Y Plot in Run Mode.

    The Go To Time option is also available when you are configuring the X-Y Plot in Design mode.

  2. Right-click on the Time Line to display a context sensitive menu.
  3. Select the Revert to Defaults option.
    The X-Y Plot disregards the Go To Time settings and reinstates the time settings that are defined in the Time Line’s configuration.

Disclaimer

ClearSCADA 2017 R2