Show and Hide the X-Y Plot Grid

You can display grid lines on the X-Axis or the Y-Axis of an X-Y Plot. The grid lines are a visual indicator that can make it easier to determine the values—you can use the grid lines to line up the values and times on the X-Y Plot.

The grid feature is especially useful when you are trying to determine the value of markers that are not positioned near to an axis.

To show the grid lines:

  1. Display an X-Y Plot in Run Mode.

    The Show Grid option is also available when you are configuring the X-Y Plot in Design mode.

  2. Right-click on the Y-Axis or X-Axis as required.
    A context sensitive menu is displayed.
  3. Select the Show Grid option.
    The horizontal or vertical grid lines are displayed (the horizontal lines are for the Y-Axis, and the vertical lines are for the X-Axis).

To hide the grid lines:

  1. Display an X-Y Plot in Run Mode.

    The Show Grid option is also available when you are configuring the X-Y Plot in Design mode.

  2. Right-click on the Y-Axis or X-Axis as required.
    A context sensitive menu is displayed.
  3. De-select the Show Grid option.
    The horizontal or vertical grid lines are hidden (the horizontal lines are for the Y-Axis, and the vertical lines are for the X-Axis).

Disclaimer

ClearSCADA 2017 R2