Configure the Y-Axis Label

You can specify a label for the y-axis. The label is a text string that identifies the axis. You specify the label's properties using fields in the Y-Axis Properties window (see Configure the Y-Axis Properties).

Use the Label section of the window to specify the properties associated with the axis label:


Disclaimer

ClearSCADA 2017 R2