Change the Appearance of the Dynagraph’s Display
You can change the appearance of a Dynagraph’s display by using the Dynagraph Properties window.
To display the window:
- Display the Dynagraph in Design mode (see Displaying an Editor).
- Right-click on the main display area of the Dynagraph (the area that will contain the traces).
A context-sensitive menu is displayed. - Select the Edit Properties option.
The Dynagraph Properties window is displayed.