Show or Hide the Title, Axes, or Key

You can choose to hide a Dynagraph’s title, axes, or key so that the remaining features on the Dynagraph resize to fill the display area.

To show or hide the title, axes, or key:

  1. Display the Dynagraph in Run or Design mode, as required (see Displaying an Editor).
  2. Right-click on the main display area of the Dynagraph (the area that will contain the traces).
    A context sensitive menu is displayed.
  3. Select or clear the relevant option (when selected, the option is prefixed with a check mark):
    • Show Title—Select this option to show the title (providing that a title has been specified for the Dynagraph). Clear the option to hide the title.
    • Show X Axis—Select this option to show the x-axis. Clear the option to hide the axis.
    • Show Y Axis—Select this option to show the y-axis. Clear the option to hide the axis.
    • Show Key—Select this option to show the key at the bottom of the Dynagraph. Clear the option to hide the key.

Disclaimer

ClearSCADA 2017 R3