Status Attributes that are Specific to Dynacard Stores
Every item in the ClearSCADA database has its own Status display (also referred to as a View window or View dialog). The Status display provides information about the status of the selected item.
Use this section if you need information on the status of the Dynacard Stores on your system.
For each set of dynacard data that is stored using a Dynacard Store, the Dynacard Store’s Status display includes a set of status attributes. For more information, see the topics that are listed in the gray footer section at the bottom of this topic. Select the relevant entry to display the topic that you require.:
Further Information
Working with Status displays: see Status Displays.