Understand the Dynagraph Display

A Dynagraph can include the following elements:

X-Axis

The horizontal axis that indicates the position of the pump in the well.

Y-Axis

The vertical axis that indicates the loading on the pump.

Key

The area at the bottom of the display that provides information about the data being shown (see Understand the Dynagraph's Key).

Markers

Small symbols (the shape of a cross, diamond, or square) that can be shown on the Dynagraph. Each marker represents an individual data reading, indicating the rod pump loading at a particular position in the well.

Traces

The lines that connect the markers together, to visually indicate the difference between the data readings.

Title

The text than can be shown at the top of the Dynagraph, to provide users with information about the Dynagraph’s content.


Disclaimer

ClearSCADA 2017 R3