Introduction to the Advanced EWS Driver

This driver is an advanced driver. It provides additional functionality to enable ClearSCADA to interface with specific supported devices using a particular protocol. To interact successfully with such devices, you need to:

Intended Audience

This guide is designed for use by engineers who are responsible for configuring EcoStruxure Web Services-specific items and features. It can also be used by system administrators when investigating any unexpected behavior relating to the Advanced EWS Driver. For more information, see EcoStruxure Web Services Specific Status Display Attributes andEcoStruxure Web Services Specific Driver Log File Options.

Document Scope

This guide explains how to configure Advanced EcoStruxure Web Services Client Driver specific features and items in the ClearSCADA database. It also describes the Advanced EcoStruxure Web Services specific statistics and diagnostics.

ATTENTION: Throughout this guide, mentions of the 'Advanced EcoStruxure Web Services Client Driver' are abbreviated to 'Advanced EWS Driver.

The Advanced EcoStruxure Web Services Driver uses a Schneider-defined standard, which allows interoperability between Schneider products and devices. ClearSCADA uses this standard to allow transfer of data between the ClearSCADA server and other Schneider applications.

The ClearSCADA Advanced EWS Driver is used to read and/or write to data on EWS servers, including:

The driver enables ClearSCADA to communicate with servers that comply with EcoStruxure Web Services version 1.1version 1.1.

For information about how to configure EWS specific features and items within the ClearSCADA database,(see Configuring EcoStruxure Web Services Devices in ClearSCADA).

NOTE: There are no driver-specific pick actions for database items on this particular driver. However, users with the required privileges can add custom pick actions to a database item by using the User Methods tab on the relevant configuration Form (see Using the User Methods Tab to Define Custom Actions in the ClearSCADA Guide to Core Configuration). See a system administrator for the documentation associated with such custom actions (also known as ‘methods’).


Disclaimer

ClearSCADA 2017 R3