Configure Logged Data Properties

The ClearSCADA Advanced EWS server retrieves and processes the Value Items values (current data) from the devices that it monitors. You can log the current data historically for point types other than String points.

Use the fields within the Logged Data section on the Point tab to specify which of this retrieved point data ClearSCADA logs historically, and which data it processes to generate alarms:


Disclaimer

ClearSCADA 2017 R3