Advanced Modbus Controller Status Attributes

If your system includes Generic Modbus controllers that do not have ‘live’ points, also see Generic Modbus Controller and Associated Channel States.

These Status attributes apply to controllers on the Advanced Modbus driver:

If your system is running an Advanced Modbus Extension Driver, refer to the relevant Advanced Modbus extension driver guide for any driver-specific status attributes that are not listed above.


Disclaimer

ClearSCADA 2017 R3