Advanced Modbus Specific Status Display Attributes

Every item in the ClearSCADA database has its own Status display (also referred to as a View window or View dialog). You view an item's Status display by selecting that item's View Status pick action or menu option. The Status display provides information about the status of the selected item, presenting the information in the form of 'status attributes'. For further information about working with Status displays, see Status Displays.

Example:

The Status display for a Generic Modbus controller provides information about the present state of that controller.

The database items that are associated with this advanced driver support a combination of:

NOTE: This section is about status attributes that are specific to this driver. In addition to the status attributes mentioned here, this driver's extension drivers might support further status attributes. For information about driver-specific status attributes that are not covered in this section, see the relevant extension driver guide.


Disclaimer

ClearSCADA 2017 R3