Common Point Properties

NOTE:This section provides information about ‘Generic’ digital points. If your system is running an Advanced Modbus Extension Driver, other types of Advanced Modbus digital point might be available. For information about non-generic Advanced Modbus digital points, see the relevant Advanced Modbus extension driver guide.

Use the fields at the top of the Digital Point tab to Configure Common Point Properties. Fields that are specific to digital points are explained below.


Disclaimer

ClearSCADA 2017 R3