System Analysis

This section is for system administrators and high-level engineers who need to use statistical and diagnostic information to assess the state of the ClearSCADA system. This section applies specifically to the Advanced Modbus driver. For more general information on analyzing a ClearSCADA system, see System Analysis.

During system analysis, you might need to:

Additionally, if a controller is not communicating with the server when it should be, see Troubleshooting.

(If your system includes Generic Modbus controllers that do not have ‘live’ points, also see Generic Modbus Controller and Associated Channel States.)

When troubleshooting on a ClearSCADA system, check the Events List for diagnostic messages. These may help to identify the cause of any abnormal conditions that ClearSCADA has detected.


Disclaimer

ClearSCADA 2017 R3